Technical FAQs

Ask a Question

What is the maximum value of the modulo logic axis with LMC078 motion controller

Maxiumum Modulo Value depends on the axis scaling factor and can be calculated as following:
 
PosPeriod * Scaling_Denom / Scaling-Num    <=   16#7FFFFFFF  
 
For example:
Scaling_Denom = 131072
Scaling-Num = 360
Max PosPeriod-Value = 5898239,997

Errors in scaling factors are shown in the Axis-configurator (in online mode) or  with below variables of  of strcuture in Axis_Ref:
Axis.uiDriveInterfaceError or
Axis.strDriveInterfaceError
Was this helpful?
What can we do to improve the information ?