Technical FAQs

Ask a Question

In M251 PLCs Is it possible to enable/disable keep alive features on modbus TCP

It is not possible to enable or disable the Keep alive feature on the default SoMachine modbus TCP server.
This feauture could be implemented by program but the user need to create his own modbus TCP server  using the CAA Net Base Services library.

 
Was this helpful?
What can we do to improve the information ?