Technical FAQs

Ask a Question

Describe M251 TCP server behaviour and keep alive

In M251 it is not possible to enable or disable the Keep alive feature on the default SoMachine modbus TCP server.
The M251 TCP Server have the following behaviour when the Client does not close the socket correctly or not keep alive message was received:

The following behaviour is the same when the PLC is in RUN or in STOP state.

1. Default configuration:
The socket will be closed after 35 seconds.
2. Using a ModbusTCP Slave Device
The socket will be closed after the configured TimeOut ( only the socket opened by the configured Master)

Was this helpful?
What can we do to improve the information ?