Technical FAQs

Ask a Question

Does Unity Pro have a cascade PID function block?

Issue: 
Cascade PID function blocks in Ecostruxure Control Expert(Unity Pro) 

Product Line:
Unity Pro, Ecostruxure Control Expert

Resolution:
Yes. There are two cascade control loop function blocks. The function blocks are PIP and PPI. The PIP consist of a PI(Proportional Integral)-master controller and a P(Proportional)-sub controller. The PPI consist of a  P(Proportional)-master controller and a PI(Proportional Integral)-sub controller.

The transfer function is as follow:

PIP
Master controller (PI- controller) --->   G(s) = gain2 x { 1 + 1/(ti x s) }
Sub controller (P- controller) --->        G(s) = gain1

PPI
Master controller (P-controller) --->   G(s) = gain1
Sub controller (PI- controller) --->     G(s) = gain2 x { 1 + 1/(ti x s) }
Was this helpful?
What can we do to improve the information ?