Technical FAQs

Ask a Question

What to do if error 2098 / 1935 occurs while installing SoMove

Do any of the following, if Error 2098/ 1935  is occurred while installing SoMove

Method-1: Clean the registry using Microsoft Fixit
1. Download and install Microsoft Fixit from the microsoft website
2. Start the Microsot Fixit to clean the registry
3. Try to install SoMove again

Method-2: Unregister and re-register the Windows Installer
1. Click the windows=> Start button, type MSIEXEC /UNREGISTER in the search box and press the ENTER key to unregister the windows installer
2. Click the windows => Start button, type MSIEXEC /REGISTER in the search box and press the ENTER  key to register the windows installer
Note: Even if you do this correctly, it may look like nothing occurred, or you may briefly see an hourglass. After you run this command, the operation is complete
3. Try to install SoMove again
Was this helpful?
What can we do to improve the information ?