Technical FAQs

Ask a Question

How can I check versions of installed DTMs ( Device Type Manager) in SoMove

From SoMove FDT (Field Device Tool) stand alone version v2.1 and onwards list of installed DTM's in the start page have been introduced.
To see list of installed DTMs, click as shown below on start page.


As a result of click, list of DTMs installed on your system and detected by SoMove FDT is displayed as below.
Note: This is example of list of installed DTMs and it in type and version may vary from user to user depending on what DTMs they have installed.
Was this helpful?
What can we do to improve the information ?