Technical FAQs

Ask a Question

Is it possible to check last device connected to SoMove

Yes, it is possible to check which was the last device that connected to SoMove.
With release of SoMove FDT standalone version v2.5 improvement made on start page that included "Last Connected Device Information"
This feature is available with SoMove FDT standalone version v2.5 and all later versions.

Information saved is as below for Last Connected Device:
- Device Type
- Reference
- Fieldbus Type
- Fieldbus address
- DTM version

For example, please check below snap for detailed understanding about how it looks.
Was this helpful?
What can we do to improve the information ?