Technical FAQs

Ask a Question

What is the part number for the cable in the VW3G48101 remote display kit?

Issue : 
Is the cable only available from the VW3G48101, remote display kit?

Product Line :
Altistart 48, ATS48

Environment :
All

Cause :
Looking to get just the RJ45 to DB9 cable only that is part of the VW3G48101 kit.

Resolution : 
The cable only is not offered as a separate component.  Order the complete kit only.
Was this helpful?
What can we do to improve the information ?