Technical FAQs

Ask a Question

How to configure load thresholds for AP4424 Switch through Web Interface.

Kindly follow the below steps to configure load thresholds for ATS Switch through Web Interface :   
1. Select the Unit tab from the navigation menu. Then select load, under Configuration in the left navigation menu.
2. Set the thresholds for total current or each bank. The configurable thresholds are Overload Alarm Threshold, Near Overload Warning Threshold, and Low Load Warning Threshold for each bank.
3. Click Apply to save your changes or Cancel to exit without saving the changes.
Was this helpful?
What can we do to improve the information ?