Technical FAQs

Ask a Question

How to set the Low Load Warning Threshold for AP4424 Switch.

The default Low Load Warning Threshold is 0 Amps, which disables the warning alarm. A 2-Amp detection threshold indicates that a circuit breaker may have tripped and activates a warning alarm. ï With a setting of 0 Amps for the Low Load Warning Threshold, the Web interface will not indicate that a circuit breaker may have tripped.
1. Select the Unit tab from the navigation menu, then select load, under Configuration in the left navigation menu.
2. Set the Low Load Warning Threshold for each bank to 2 Amps.
3. Click Apply to save your changes or Cancel to exit without saving the changes."
Was this helpful?
What can we do to improve the information ?