Technical FAQs

Ask a Question

Do we have DTM for ATV310 drive in Somove ?

ATV310 is an Easyline offer and there is no DTM available for it and it is not available on SoMove as well.It has RS485 port for Modbus communication with other devices.
Was this helpful?
What can we do to improve the information ?