Technical FAQs

Ask a Question

what is the Motor Choke reference for ATV630 Drives ?

We do not have any motor choke available in ATV630 catalog and we never have done any test with ATV630 and motor choke. One may refer dv/dt or sinus filter for long motor cables. References are given in the catalog.
Refer below link for catalog.


https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=DIA2ED2140502EN+%28web%29.pdf&p_Doc_Ref=DIA2ED2140502EN
Was this helpful?
What can we do to improve the information ?