Technical FAQs

Ask a Question

what are the factors which determines the life expectancy of power capacitors?

The factors are:
1.) Maximum Permissible Voltage.
2.)Maximum Permissible Current.
3.) Maximum Temperature.
4.)Number of switching operations.
Was this helpful?
What can we do to improve the information ?