Technical FAQs

Ask a Question

What is the maximum number of BMENOP0300 modules that can be mounted on a local rack of M580 CPU?

The maximum number of BMENOP0300 modules that can be mounted on a local rack is determined by your choice of CPU.
The maximum numbers of communication modules, including BMENOP0300 modules, supported by M580 CPUs are as follows: 
 
CPU Maximum Number of Communication Modules
BMEP581020 2
BME•5820•0 2
BMEP5830•0 3
BME•5840•0 4
BMEP585040 4
BME•586040 4
Was this helpful?
What can we do to improve the information ?