Technical FAQs

Ask a Question

How can I calculate messaging rate for Modbus Servers?

The messaging rate can be calculated as follows:
Messaging Rate = ((1/ Message Sampling period) x Objects
This formula includes the following elements:
Element Description
Messaging Sampling period The interval at which messages are processed
Objects The number of devices, either client or server, that are actively communicating
Was this helpful?
What can we do to improve the information ?