Technical FAQs

Ask a Question

How can I get the Default IP Address of BMX NOR 0200 H Module?

You get the Default IP Address of BMX NOR 0200 H Module from it's MAC Address.

The default IP address format is 84.x.y.z:
  • 84: a fixed value
  • x.y.z: The last three fields in the default IP address correspond to the decimal equivalents of the last three bytes in the MAC address.
Example:

For example a device with 00-00-53-12-01-C4 MAC address has the following default IP address: 84.18.1.196 (12 hex = 18 dec, 01 hex = 1 dec, C4 hex = 196 dec)
Was this helpful?
What can we do to improve the information ?