Technical FAQs

Ask a Question

Where can I find the TM3TI4D Module in Somachine Software?

The TM3TI4D Add-On is delivered as a container file in SECO format and can only be installed after installing SoMachine V4.3. Use the SoMachine Configuration Manager (SCM) to install this Add-On.

In Windows Explorer, double-click the SECO file delivered through this Add-On, which will start SCM and the installation. Alternatively, you can start SCM manually by selecting the tab "Add-Ons/Patches" and choose "From File >" to open the SECO file.

Note: The installation of the TM3TI4D Add-On requires administrator privileges to start.

Was this helpful?
What can we do to improve the information ?