Technical FAQs

Ask a Question

Where to find the driver reference help in CitectSCADA 2016?

Each driver, whether it is installed with Citect SCADA or as part of a driver pack, is supported by the Driver Reference Help.

The Driver Reference Help is located in the bin directory:

<install drive>\Program Files (x86)\Schneider Electric\Citect SCADA 2016\Bin

You can also access it from the Windows™ Start menu:

Start | All Programs | Schneider Electric | 2016 2016 | Driver Reference Help
Was this helpful?
What can we do to improve the information ?