Technical FAQs

Ask a Question

Does LXM32 series is compatible in in radioactive / nuclear environment?

In principle, the motors and LXM32 are not suitable for use in radioactive environments.
Machine solution products do not comply with the nuclear safety standard IEC 61513.
Was this helpful?
What can we do to improve the information ?