Technical FAQs

Ask a Question

What is terminal tolerance of LC1F630 Contactor

The tolerance value on distances between the terminals of LC1F630 are given as follows: 80+/-1 and 264+/-1.8.
Was this helpful?
What can we do to improve the information ?