Technical FAQs

Ask a Question

What is the ambient operating temperature for Acti 9 Smartlink (ethernet) for horizontal and vertical mounting position

The ambient operating temperature is for Acti9 Smartlink (ethernet):

 Horizontal mounting: −25°...+60°C
 Vertical mounting: −25°...+50°C
Was this helpful?
What can we do to improve the information ?