Technical FAQs

Ask a Question

Whether third party servomotors can be used with LXM32 servo drives?

Third party motors are only possible via an additional analog encoder module or resolver module on slot 2 on Lxm32M and the motor encoder should only be resolver or sincos.
Was this helpful?
What can we do to improve the information ?