Technical FAQs

Ask a Question

Is it possible to use XCE145 to replace XCE146.

The XCE146 is with a steel roller lever instead of the thermoplastic roller lever (difference).
The XCE145 is with the thermoplastic roller lever.
Yes, it is possible to replace XCE146 by the XCE145 if the plastic roller is acceptable for his application. This is the same reason for all the limit switch series, we can propose thermoplastic roller, steel roller and sometimes steel roller with ball bearing.
Was this helpful?
What can we do to improve the information ?