Technical FAQs

Ask a Question

What is the part number of cable for XX7V1A1PAM12 which is 5m or more.

There are 5 m and 10 m cable; below are the part number:---
5-meter cable (Straight)=> XZCP1141L5
5-meter cable (Elbowed)=> XZCP1241L5
 
10-meter cable (Straight)=> XZCP1141L10
10-meter cable (Elbowed)=> XZCP1241L510
Was this helpful?
What can we do to improve the information ?