Technical FAQs

Ask a Question

Why both cpu of M580 hot standby boot up in wait mode?

Possible cause:
Both the CPU rotary switch are selected (from the backside of the cpu) either in A, B or in Clear position.  

Possible solution:
Select one of the CPU rotary switch in A & other in B position.
Was this helpful?
What can we do to improve the information ?