Technical FAQs

Ask a Question

what is the Maximum length of Modbus serial RS485 bus without branching for M340 CPU serial port.

The Maximum length of Modbus serial RS485 bus without branching is 1000 meters and 15 meters with branching.

 
Was this helpful?
What can we do to improve the information ?