Technical FAQs

Ask a Question

How many BMXNOM0200 module can be installed with BMXP342000 CPU module.

BMXP342000 CPU supports 36 expert channels means we can use 36 modbus ports for communication. 
 
NOM modules consumes 2 expert channels as there are 2 modbus ports on it. So with this cpu, we can use maximum 18 modules 

On per channel we can connect 32 serial devices.

 
Was this helpful?
What can we do to improve the information ?