Technical FAQs

Ask a Question

What happens to the SF6 gas after it is recovered.

There are several options according to the quality of the recovered SF6 and the SF6 regeneration possibilities existing in any country. In most cases it is sent to a recycling centre where it is regenerated by passing continuously through various special filters. If this is not possible, it is sent to a destruction centre for incineration.
Was this helpful?
What can we do to improve the information ?