Technical FAQs

Ask a Question

Is it possible to use other HMI software on the Magelis line of iPC?

Issue:
Is it possible to use other HMI software on the Magelis line of iPC?

Product Line:
Magelis iPC

Resolution:
Yes, it is possible to use other 3rd party HMI software on the Magelis line of iPCs. Just ensure that the Operating System and Hardware meet the minimum requirements of the HMI software. Note that any issues with the 3rd party HMI software are not Schneider Electric's responsibility. Please contact the support of the 3rd Pary HMI software if issues arise.
Was this helpful?
What can we do to improve the information ?