Technical FAQs

Ask a Question

Video: How to read the data in the Profibus DP Diagnose of a PRM by M580?

Goals and Symptoms
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?

Facts and Change

TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212.

Causes and Fixes

The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to configure a Profibus slave (in this case a STBNDP2212) and read the data in the Profibus DP Diagnose Service using the PRM RDIAG function block.
 
Was this helpful?
What can we do to improve the information ?