Technical FAQs

Ask a Question

What are the Supported services in DeviceNet protocol in VAMP relay

In VAMP relay Vamp 50,Vamp 200, Vamp300 , Supported services for data model objects are only Set Attribute Single (SAS) and Get Attribute Single (GAS).
GAS service is available for all attributes with the GET or GET | SET access type and the SAS service is available for all attributes with the GET | SET or SET access type.
Was this helpful?
What can we do to improve the information ?