Technical FAQs

Ask a Question

How Analog measurements are transferred in IEC-103 protocol in Vamp 255 relay

Analog measurements are transferred in two different formats in IEC-103 protocol. Value
format is depended on application message type, ASDU. The following ASDU types are available for measurement values: 
refer the attachment
Was this helpful?
What can we do to improve the information ?