Technical FAQs

Ask a Question

How measurements are sent in regular interval in IEC103 protocol in Vamp255 relay.

Measurements are sent in regular intervals. The ‘MeasInt’ setting defines a delay between two analog value messages and can be used for limiting bus traffic. 
Was this helpful?
What can we do to improve the information ?