Technical FAQs

Ask a Question

How to log on to WorkStation as another Windows user in EcoStruxure Building Operation.

Below is the procedure to log on to workstation as another windows user:
  1. In WorkStation, in the User name box, type the name of the Windows user account you want to use to log on.

  2. In the Password box, type the Windows password for the user account.

  3. In the Domain box, type a Windows domain name. If you do not enter a domain name, you are logged on to the local domain as an EcoStruxure Building Operation User.

  4. Select the HTTPS protocol option for communication with the EcoStruxure BMS server.

  5. In the Server box, enter an EcoStruxure BMS server name or an IP address.

  6. Select Remember me on this computer to have WorkStation remember your settings.

  7. Click Log on

Was this helpful?
What can we do to improve the information ?