Technical FAQs

Ask a Question

How to configure a custom audible alert for an alarm to play an audio file when the alarm is triggered in Ecostruxure Building Operation.

​1.In WorkStation, expand the EcoStruxure BMS server where the alarm is to be played.
2.In the System folder, select the Audio folder and ensure the audio file has been added.
3.Select the alarm for which you want to configure the custom audible alert.
4.Click the Presentation tab of the alarm.
5.Select Audible alert .
6.In the Custom audio box, enter the path of the audio file you want to use.
7.Click the Save button

Was this helpful?
What can we do to improve the information ?