Technical FAQs

Ask a Question

What are the different Alarm Types which can be configured in an EcoStruxure Building Operation

There are different types of alarms that handle different types of variables and different forms of evaluation. Below are the alarm types in an EcoStruxure Building Operation:
  • Change of State Alarms 
  • Out of Range Alarms 
  • Out of Reference Range Alarms 
  • Multistate Alarms 
  • Matching Text String Alarms 
  • Variable Status Alarms 
  • Sum Alarms 
  • Enumeration Alarms 
  • System Alarms 
  • EcoStruxure Web Service Alarm Item
Was this helpful?
What can we do to improve the information ?