Technical FAQs

Ask a Question

How to configure Xenta Server (Xenta 511, 527, 555, 701, 711, 721, 731, 913) for automatic login.

Some customers may specify that the login screen to a Xenta Server be bypassed. The steps are described below:

1. Configure the user you want to automatically log in to the Xenta Server

2. Generate a certificate to avoid having the certificate error pop up every time you connect to the Xenta Server, go to XBuilder, and generate a certificate that has the same name as the IP address of the Xenta Server.

3. Edit Slogin.html and loggedout.html
- Connect to the Xenta Server using FTP
ftp://XXX.XXX.XXX.XXX
- The Slogin.html and loggedout.html are located in the folder www/index
Copy the files to your local hard drive
- Edit the files with, for instance, notepad and change the following
Slogin.html
Line 54
document.AuthForm.UserID.focus();"
document.AuthForm.UserID.focus(); send(AuthForm);"
Line 98
input type="text" name="UserID" value="" size="20" >
input type="text" name="UserID" value="user" size="20" >
Line 104
input type="password" name="PassWord" value="" size="20">
input type="password" name="PassWord" value="password" size="20">
loggedout.html
Line 5 (extra line, add < symbol at beginning of line)
meta http-equiv="refresh" content="2;url=/www/index/Slogin.html">

4. Carry out the changes
- Reconnect to the Xenta Server using FTP
- Change the names of the files that are already in the Xenta Server (Backup)
- Copy the files that from your hard drive to the Xenta Server
Was this helpful?
What can we do to improve the information ?