Technical FAQs

Ask a Question

Video: How is an external fault function set up on the ATV212 drive?

Issue:
Video: How is an external fault function set up on the ATV212 drive?

Product Line:
Altivar 212

Environment:
All

Cause:
Configuration for Drive response to External Fault condition.

Resolution:
To set an external fault function you will need to program one of the logic inputs F/R/or RES as external fault.
Under F--- menu.
F111 is F
F112 is R
F113 is RES terminals.

Let's assume you want to program R as external fault function:
Set F112 to 11 for external fault where OFF is no detected fault, and ON is where motor stops according to method set by parameter [Ext fault stop mode] (F603).  
This will prompt E on display if external fault is on.
F603 options: 0 for freewheel, 1 for ramp stop, 2 for DC braking stop.

 
Was this helpful?
What can we do to improve the information ?