Technical FAQs

Ask a Question

Do the PME 9.x Activation IDs work for a PME 8.x system?

Issue
Do the PME 9.x Activation IDs work for a PME 8.x system?

Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 8.x


Environment
Activation IDs

Cause
Are the PME 9.x activation IDs backwards compatible.

Resolution
The PME 9.x activation IDs are backwards compatible with PME 8.x.
 
Was this helpful?
What can we do to improve the information ?