Technical FAQs

Ask a Question

Can the stop button on the HMI be disabled as an Estop when in terminal control mode?

Issue:
Can the stop button on the HMI be disabled as an Estop when in terminal control mode? 

Product Line:
ATV212 ,  SFD212 , SFD21 

Environment:
All serial numbers 

Cause:
Prevent "Flashing E" code. Prevent having to cycle power to clear the drive. 

Resolution:
Stop/reset key.
The setting of parameter F734 determines whether it is possible to stop the drive by the Stop key which is located on the drive and graphic display option.
0 = [Enable]    1= [Disable]   

Note: 
LOSS OF CONTROL
You are going to disable the stop button located on the drive and graphic display option. Do not select 1 unless exterior stopping methods exist. 
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Was this helpful?
What can we do to improve the information ?