Technical FAQs

Ask a Question

How can you change the configuration of the Momentum CPU Serial port 1 from RS485 to RS232?

 Issue:
 
When I try to change the Serial Port on the Momentum CPU from RS485 to RS232, the configuration is grayed out in Control Expert (Unity Pro).
 
Product Line:
Momentum PLC 
 
Environment:
Control Expert v14
Unity Pro XL V13
 
Cause:
The serial port can not be changed from RS485 to RS232.
Resolution:
 Serial Channel 1 on the Momentum CPU modules 171 CBU 78090, 171 CBU 98090 and 171 CBU 98091 is a static RS485 port.
It is not configurable to be used with RS232.
Was this helpful?
What can we do to improve the information ?