Example of structured text logic program to insert values into a data table
DISCLAIMER
This sample program is intended to demonstrate one or more programming functions or methods and is presented as programming example only. Schneider Electric assumes no liability for the use or application of this example program or any portion thereof.
This small logic program reads data from 3 database points named String, Point 1 and Point 2, and inserts this data into a custom table in ClearSCADA named CSTable1.
PROGRAM InsertIntoTable
VAR
sWriteString AT %M(.String): STRING[250];
sWriteValue1 AT %M(.Point 1): DINT;
sWriteValue2 AT %M(.Point 2): DINT;
END_VAR
VAR NOCACHE
vSQLWrite AT %D(INSERT INTO CSTable1 VALUES (?,?,?))WITH_PARAMS sWriteString, sWriteValue1, sWriteValue2;