Technical FAQs

Ask a Question

Using Modbus to trigger a Waveform Capture on a CM2000

Product Line
CM2000 series meter

Environment
Modbus Register Writes

Resolution
In order to trigger a waveform capture, it will be necessary to use Modbus Command Writes to trigger the waveform capture.

Using Modbus Tester (or another Modbus read/write program):

Write the value 4913 to register 7700.
Write the value 1 to register 7701.
Write the value 28120 to register 7702.
Was this helpful?
What can we do to improve the information ?