Technical FAQs

Ask a Question

Where can I download Power Monitoring Expert 9 installation file?

Issue
Looking for Power Monitoring Expert 9 install file

Product
Power Monitoring Expert 9

Environment
Software Installation Files

Resolution
PME 9 (ISO) software can be found at the Schneider Electric Box links below: Note that healthcare and Data Center modules are included in the installer and require licenses. 

https://schneider-electric.app.box.com/s/fg6vepjfbiyncvpy4nawgoc7clk6672l

Instructions to verify a successful download have changed. Please make sure to read the instructions before running the installer.

For documentation of PME 9, refer to article FA358303
Was this helpful?
What can we do to improve the information ?