Technical FAQs

Ask a Question

What does the triangle LED on the ATV320 drives indicate?

 Issue:
Customer sees the triangular LED is on.  Wants to confrim what this indicates.

Product line:
Altivar Machine ATV320 Altivar 320

Environment:
all

Cause:


Resolution:
When the triangle LED is on, the Drive is in a Fault condition.  Check the display for the fault code to troubleshoot. 
The LED goes off when the fault is cleared and the drive has been reset.
Was this helpful?
What can we do to improve the information ?