Technical FAQs

Ask a Question

ION9000: Maximum number of option modules

Issue
Is there a maximum number of option modules that could be installed on ION9000 meter?

Product Line
ION9000

Environment
Digital/Analog Input/Output Option Modules
 
Cause
The optional I/O available on ION9000 and limitation.

Resolution
  • The maximum number of option modules supported by the device is four. However, there are limitations.
  • Depending on the type and quantity of option modules attached to your meter, you may need to reduce your meter’s maximum operating temperature or limit the number of option modules.
**Warning: EQUIPMENT DAMAGE. Do not exceed the maximum number of option modules. Failure to follow these instructions can result in equipment damage

The maximum operating temperature for option modules is as follows:
 
 
Maximum operating temperature
PM89M2600
Digital (2 out, 6 in)
PM89M0024
Analog (2 out, 4 in)
70 ºC (158 ºF)
0 - 4
0,1
70 ºC (158 ºF)
0
2
60 ºC (140 ºF)
1,2
2-4
Was this helpful?
What can we do to improve the information ?