Technical FAQs

Ask a Question

What is the Ingress protection of our Hexa Meter

The Ingress protection of  EM6433H is :

Front IP51 (IP54 w/ gasket),
Rear IP30 - as per IEC 60529
Was this helpful?
What can we do to improve the information ?