Technical FAQs

Ask a Question

What If Energy meter showing wrong values in SBO over the Modbus protocol during configuration.

Follow the below steps.
1. Login to the workstation.
2. Select the Energy Meter parameter.
3. Select the proper "Register Type"
4. Issue will be resolved.
See the attached snapshot for your reference.
 
Was this helpful?
What can we do to improve the information ?