Technical FAQs

Ask a Question

How much is the Voltage Drop in ATV71 and ATV930

Voltage drop for ATV930  and ATV71 on nominal load is about 4% and with AFE is about 2.5%.
 
Was this helpful?
What can we do to improve the information ?