Technical FAQs

Ask a Question

How to find the IP address of controller in Citect Scada 2016

Open the topology in Citect scada and select Components & Menu from tool bar. Above the row, there is board and select port in place of board from drag down menu. IP address is available there. For more details refer the attachment.
 
Was this helpful?
What can we do to improve the information ?